Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
L99ASC03 Fully-Integrated Motor Driver IC for Three-Phase Brushless Motors Slide 12

Shown here is the waveform of the terminal voltage and the back-EMF. The back-EMF information can be extracted from the terminal voltage of the floating phase. From T1 and T2, the winding is floating, from T2 and T3, the winding is conducting current and from T3 to T4, the winding is floating again. The engineer can get the back-EMF signal when PWM is “off”. If the back-EMF is negative, it is clamped by the diode paralleled with the switch. Between T1 and T2, rising edge of zero crossing is detected, and between T3 and T4, falling edge of the zero crossing can be detected. The red curve is the full shape of back-EMF. When executed for all three phases, the engineer will have the full back-EMF waveform.

PTM Veröffentlicht am: