Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
L99ASC03 Fully-Integrated Motor Driver IC for Three-Phase Brushless Motors Slide 10

To illustrate the function, the engineer will do some circuit analysis. Shown here is the circuit model when the current is freewheeling. From the circuit, Vc=Vn+Ec, and Vn can be calculated from phase A and phase B. From phase A there is one equation, and from phase B there is another. Putting them together, one gets Vn=Ec/2. Therefore, Vn essentially is half the voltage of Vc, which is the back-EMF on the phase C winding.

PTM Veröffentlicht am: