Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
L99ASC03 Fully-Integrated Motor Driver IC for Three-Phase Brushless Motors Slide 16

So what goes into the L99ASC03? Integrated into one chip, there is a Low Dropout Regulator, three half-bridge drivers for the six MOSFETs that drive the motor, a programmable current sense amplifier, built in advanced back-EMF detection with diagnostics, control logic for Diagnostics and Protection, and SPI communication interface with the host microcontroller.

PTM Veröffentlicht am: