Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
healthcare-wellness-slide17

The features of the L1 series of STM8L and STM32L, from entry level to the feature-rich 32-bit ARM Cortex-M3 devices are shown on this slide. For the STM8L devices these include: an 8-bit MCU with up to 16 MIPS at 16MHz; 2 to 64kbytes of embedded Flash, up to 4kbytes of SRAM and up to 2kbytes of EEPROM; up to four low-power modes, as low as 350nA with SRAM and context retention; run mode dynamic consumption down to 150μA/MHz; and a free touch-sensing library. Likewise, the features of the L1 series STM32L includes: a 32-bit ARM Cortex-M3 with up to 33 DMIPS at 32MHz; pin-to-pin compatibility with STM32F series (except VBAT); 32 to 384kbytes of embedded Flash, up to 48kbytes of SRAM and up to 12kbytes of data EEPROM; six low-power modes, as low as 300nA; low-power dynamic modes enabling low-power run down to 9µA, low-power sleep down to 4.9µA with one timer; and economical run mode consumption as low as 230μA/MHz from Flash at zero-wait state with dynamic voltage scaling (three ranges).

PTM Veröffentlicht am: