Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
ML610Q100-Slide5

These devices are offered in small packages, that do not require external capacitors or crystals for voltage regulation or as a timing reference. Even without an external crystal, or any other components, the time base of these devices are accurate up to 1%. Some of the devices have on chip FLASH that can be used to store data, so there is no need for external EEPROMs or related devices for data logging.

PTM Veröffentlicht am: