Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
ML610Q100-Slide19

To meet the goal of reducing external components, the LCD bias voltage function on the ML610Q17x devices do NOT required external resistors or capacitors, as they typically would for other devices with LCD bias voltage generation. This frees up two pins as GPIO and reduces external component count. The PWM modules can be used for driving analog functions like IGBTs that would control the power to heating elements in a small appliance or industrial heater.

PTM Veröffentlicht am: