Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
ML610Q100-Slide25

The LAPIS development kit consist of a board, sample projects, a PC based GUI, a nanoEase debugger, and the complete IDE. The nano EASE communicates with the Debugger software on the PC through a USB interface to control and monitor the microcontroller while it is operating. The PC based GUI communicates to the board over another USB interface from a computer. The GUI interacts with a program on the microcontroller so that the user can select functions on the device and configure and manipulate them. For example the user can select a specific IO pin as an output and write a value to it. This can all be done without the designer writing any code so a quick evaluation can be done.

PTM Veröffentlicht am: