Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
ML610Q100-Slide20

A typical application for this type of device would be a small home appliance that requires an LCD display for user interface and a controlled heating element. Typically a designer would want to modulate control of IGBTs to moderate the heating element. The two PWM modules on these devices are ideal for that type of control. The SA type ADC could be used for monitoring the temperature.

PTM Veröffentlicht am: