Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
MAX11300 Programmable Mixed Signal IO - Pt 1 Slide 9
DAC operations can be monitored using an internal auxiliary ADC for correction and calibration purpose. In such a mode, the ADC samples the DAC-configured ports to allow the host to monitor that the voltage at the port is within expectations given the accuracy of the ADC and DAC. When this mode is used both DAC and auxiliary ADC would use the same referenced voltage.
PTM Veröffentlicht am: