Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
MAX11300 Programmable Mixed Signal IO - Pt 1 Slide 11
By combining GPI- and GPO-configured ports, unidirectional level translator paths can be formed. The signaling at the input of the path can be different from the signaling at the end. For example, a unidirectional path could convert a signal from 1.8 V logic level to 3.3 V logic level. The unidirectional path configuration allows for the transmission of signals received on a GPI-configured port to one or more GPO-configured ports.
PTM Veröffentlicht am: