Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
PowerWise Products and Technology Slide 9
The goal of a subsystem is to actively reduce the power consumed beyond that of reducing passive power consumption (i.e. the energy consumed by the devices alone). Using lower power devices is good, but the subsystem approach takes that to even a higher level of savings. Subsystems can also be created with digital signals to assist processors in evaluating the current state. For example, cable disconnect detection on a cable driver can feed information back to a digital core to disable other sections of the system when that output is no longer in use. This can be highly useful on switches or other devices with many outputs – in many cases, not all the outputs are in use. Additionally, many subsystems can work autonomous from a CPU or digital core and still provide feedback on the current state, acting in near real time off-loading the processor or FPGA while maintaining very high response times.
PTM Veröffentlicht am: