Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
PowerWise Products and Technology Slide 6
An example calculation is shown here for a high speed analog to digital converter. Here the calculation uses the power consumed while converting an AC analog signal at the maximum rate of the converter. The device shown is the ADC12EU050 which yields an efficiency rating of 0.48 pJ per conversion. The “per conversion” part of the metric is a result of the effective number of bits at frequency or the real measure of the performance of the data converter. The limit is 2.5 pJ/conversion, which places this device well inside the limit specification.
PTM Veröffentlicht am: