Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
PowerWise Products and Technology Slide 24
In an open-loop system, a voltage regulator supplies a fixed voltage to a core of an ASIC or SoC. In a close-loop AVS system, a Hardware Performance Monitor, or HPM, is embedded in the ASIC to monitor the process and temperature variation of the core. This information is communicated to the Advanced Power Controller (APC) to determine if there is a voltage optimization that can be done. The voltage optimization is then communicated to the Energy Management Unit (EMU) through the PWI interface. The EMU then closes the loop by supplying the most optimized voltage back to the core of the ASIC.
PTM Veröffentlicht am: