Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
MAX31856 Precision Thermocouple to Digital Converter with Linearization Slide 9
The MAX31856 is a sophisticated thermocouple-to-digital converter with a built-in 19-bit analog-to-digital converter (ADC). Internal functions include correction for thermocouple nonlinearity, input protection, cold-junction compensation sensing and correction, a digital controller, a SPI-compatible interface, and associated control logic. The temperature conversion process consists of five steps: The input amplifier and ADC amplify digitize the thermocouple’s voltage output. The internal temperature sensor measures  the cold-junction temperature. Using the internal lookup table (LUT), the ADC code corresponding to the cold junction temperature for the selected thermocouple type is determined. The thermocouple code and the cold-junction code are summed to produce the code corresponding to the cold-junction compensated thermocouple temperature. Finally, the LUT is used to produce a cold-junction compensated output code in units of °C. However, the MAX31856 users do not need to worry about all of that, as it is done automatically.
PTM Veröffentlicht am: