Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
MAX31856 Precision Thermocouple to Digital Converter with Linearization Slide 15
Shown here is the GUI reading for a K-type thermocouple at room temperature. To gather data the engineers starts with the Configuration tab and selects “Auto Convert”. Next in the Status tab the engineer selects “Auto polling” and the graph will have a continuous display for both the Thermocouple temperature and the Cold Junction Temperature (as measured by the on-chip temp sensor).
PTM Veröffentlicht am: