Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
MAX31856 Precision Thermocouple to Digital Converter with Linearization Slide 6
The upper chart here shows the output voltage vs. temperature for a type K thermocouple. The curve is reasonably linear, although it clearly has significant deviations from absolute linearity. The lower chart shows the deviation from a straight-line approximation, assuming a linear output from 0°C to +1000°C for an average sensitivity of 41.28 μV/°C. In practice, linearity correction can be done by calculating the actual value or by using a lookup table which maybe a throughput issue with slower MCUs.
PTM Veröffentlicht am: