Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
mech spec
The open frame product family comes in an industry standard 3x5” footprint with a low 1.58” profile that is compatible with 1U requirements. This includes the baseplate that can be used for conduction cooling. The fully enclosed with fan models have a 3.15 x 5.83” footprint while keeping the profile down to 1.60”. Every effort was made during the design to keep the enclosed with fan length below 6 inches for space critical requirements. The aux connector pinout has no pin for #9 to eliminate accidental reversing of the cable assembly in a production environment.
PTM Veröffentlicht am: