Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
Embedded Systems Troubleshooting with Oscilloscopes Slide 9

Shown on this slide is a trigger set up example. The yellow carrot in the horizontal axis is the trigger point and can be seen immediately following ID 400. That is because the trigger was requested on ID 400 hexadecimal in 11-bit format. The bit rate for CAN is displayed also, which on this particular frame or capture is at 125 kbit/s.

PTM Veröffentlicht am: