Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
Embedded Systems Troubleshooting with Oscilloscopes Slide 3

Serial decoding is working with a string of ones and zeros, typically, and converting the strings of ones and zeros to hexadecimal format. Before decoding became popular in oscilloscopes, the engineer would have to count the bits, actually capturing the waveform data and then counting the bits. Once the bits were counted, the engineer would convert that binary information into hexadecimal with the assistance of a scientific calculator. This was time consuming and very prone to errors. Shown on this slide, the top row of ones and zeros is the binary byte and the decoded hex values are shown below.

PTM Veröffentlicht am: