Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
Embedded Systems Troubleshooting with Oscilloscopes Slide 2

It is important to understand what an embedded controller is. Typically these are 8-bit, 16-bit, or 32-bit microcontrollers. They consist of memory devices and mixed signal devices; anything shown in the gray blocks on this slide are mixed signal devices, meaning they could have analog and digital waveforms present. The green blocks indicate analog devices and the red blocks are digital. The microcontroller will have both analog and digital signals present at the same time. One microcontroller can have multiple serial protocols such as I²C, SPI, UART, CAN bus, LIN bus signals, and more.

PTM Veröffentlicht am: