Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
Embedded Systems Troubleshooting with Oscilloscopes Slide 8

The oscilloscope has the ability to do serial triggers, and can trigger on an ID. For example, in CAN bus specifically it can decode 11-bit or 29-bit. It is able to trigger on a data value, equal to a value, range, out-of-range and so on. It is also able to trigger on remote frames, or trigger on error frames. These triggering controls vary from protocol to protocol; they are not all exactly the same.

PTM Veröffentlicht am: