Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
GWS250-Slide3

The output voltage can be remotely turned ON and OFF using the CNT terminals. Apply a voltage or leave the CNT terminals open circuit to inhibit, turn OFF, the output. To turn the output ON, pull low or short with a closed contact to enable the output voltage. The GWS is shipped from the factory with the CNT terminals jumpered to allow immediate use.

PTM Veröffentlicht am: