Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
GWS250-Slide10

The GWS250 can be used in equipment that needs to meet either Energy Star in the US or the European ErP/EuP requirements for standby power, as the unit is specified to draw less than 0.5W. In this condition the output is inhibited using the remote ON/OFF feature. Of course, no power is being pulled from the standby output at this time. Even when the output is enabled, the offload power draw is only 6W.

PTM Veröffentlicht am: