Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
GWS250-Slide12

The GWS250 has PFC, Power Factor Correction, circuitry allowing it to meet the European standard IEC 61000-3-2. The plot on this slide shows that the series not only meets Class A, which is used for professional equipment, but also the tougher Class C standard that applies to lighting equipment. Again the series will pass even at 25% load.

PTM Veröffentlicht am: