Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
iNemo Slide 12

This slide discusses the API that was previously shown in the block diagram. Users may want to familiarize themselves with quaternions. There are some good videos available to provide a good sense of what is involved with the complex numbers. Another output is the heading, pitch, and roll. Sometimes the terms will be shown as yaw, pitch, and roll; the yaw is also known as heading. Linear acceleration is provided with the gravity, the 1g offset, removed. There are many applications available for an iPhone or a smartphone, Android-based, or other, that can be downloaded to read the linear acceleration, going through filtering to remove gravity. These functions are what are output by Sensor Fusion. A header file will be generated and the user can call functions requesting quaternions, heading, and linear acceleration; the API will provide the requested data.

PTM Veröffentlicht am: