Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
How to Easily Design a Stepper Motor Slide 4

To make the motor revolve the key parameter is the torque which is the force applied to the shaft. But how the force is generated? A current flowing in an inductance or coil creates an electromagnet. The characteristics of the magnet depend on the current intensity and the direction. Two magnets will attract each other, north and south poles attract each other. The force to attract two magnets depends on the strength of the magnetic field, that depends on the current flawing through the coil. Therefore, in any condition, the torque will depend on the current. In other words, the amount of current controls the torque of a motor.

PTM Veröffentlicht am: