Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
How to Easily Design a Stepper Motor Slide 20

Thanks to the SPI, the devices can be put in a daisy chain configuration. This is very useful in the cases such as to limit the number of pins required from the microcontroller, only one CS is used; and to synchronize motors. If several motors must perform some tasks simultaneously, thanks to the daisy chain, when the CS is released all the motors will perform the command at the same time. Daisy chaining can be performed with all the L647x family, and combinations of an X number of L6470 can be put in daisy chain with y number of L6474 and z number of L6472.

PTM Veröffentlicht am: