Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
How to Easily Design a Stepper Motor Slide 15

The complexity is dramatically reduced by the EasySPIN L6474.  T_Fast is the maximum time for the fast decay when the current is stable and T_fall_step is the maximum time to decrease the current level. The EasySPIN will apply a fraction of this timing depending on the position in the sine wave. The values also depend on the minimum ON time and the minimum OFF time, that are defined with the ripples accepted in the system.

PTM Veröffentlicht am: