Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
How to Easily Design a Stepper Motor Slide 13

With competitors’ solutions, the timing of decay modes must be programmed with external RC circuits. With the L6474, all of the values are in a register that can be read or written by the microcontroller through an SPI bus (addresses h0E, h0F and h10). The current is also programmed with the TVAL value (h09 address).

PTM Veröffentlicht am: