Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
Environmental Sensors Roadmap Slide 6
The features shown on this slide can be used as a first pass check to determine if the LPS25 and or LPS331 will fit the customers application. The key parameter is the operating range (260 to 1260 mbar) which is the atmospheric range.
PTM Veröffentlicht am: