Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Spa-Slide5
The IEC61000-4-2 standard addresses ESD events seen in the field or at the system level. As shown in the schematic, a 330 Ohm resistor is used to discharge the capacitor so the currents injected into the device being tested are much higher than the previous MIL-STD model. All manufacturers of electronic equipment will use this ESD standard to evaluate their devices so in most all cases IC’s will require external ESD protection as the currents in this model are more than five times greater than the previously discussed.
 
PTM Veröffentlicht am: