Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List

Spa-Slide3

ESD is the result of electron transfer when two materials make contact and then separate or what is known as triboelectric charging. The level at which static electricity can build up is determined by several factors such as area of contact, the speed of separation, relative humidity, and chemistry of the materials. Some common examples of static generation are walking across carpet or picking up a poly bag from a work bench. These types of events can generate charges from thousands of volts to tens of thousands of volts in a normal environment.
 
PTM Veröffentlicht am: