Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List

Spa-Slide10

Ultimately, the external ESD protection device reduces the amount of energy the IC must dissipate. Limiting that energy is the result of choosing the ESD device with the appropriate turn on voltage and the one that will present the lowest impedance to GND during a transient. These key parameters along with many others will now be discussed.
 
PTM Veröffentlicht am: