Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List

Spa-Slide15

The peak pulse current is the maximum current the protection device can withstand. It has a wave shape that is derived from standards pertaining to lightning immunity and also an important aspect for devices that are mostly geared towards protecting telecom equipment from induced lightning surges. Often TVS diode array datasheets will show current levels with a wave shape following them such as 8 by 20 or 2 by 10. This is simply stating the rise time and fall time to 50% of it’s peak as shown in the plot to the left. These are also the same currents used to test for clamping voltage because the longer µs rise times help avoid issues with parasitic inductance.
 
PTM Veröffentlicht am: