Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
digital-power-slide11

The PowerNavigator software provides a PowerMap rail block for a quick overview of each DPM attached to the system. In the monitor view, the default view of each of the DPM parameters are shown, from primary channel bus voltage, current, power, and temperature. The Rail Inspector page, accessible by double clicking on the rail block, allows the digital power monitor registers to be easily configured, including ADC timing, external timing, setting alert thresholds, and SMB alerts. PowerNavigator is an excellent tool when working with multiple digital power devices (not just DPMs).

PTM Veröffentlicht am: