Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
power-switch-slide9

In a double pole, double throw switch, the user can turn the power on and off and choose between two settings. An example of a double pole, double throw switch is a blow dryer. When the unit is turned on, both the fan and heater are turned on at the same time. The user will decide if they want it on low or high fan with low or high heat.

PTM Veröffentlicht am: