Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
power-switch-slide6

In a single pole, single throw switch, the circuit is complete when the switch is actuated, as the diagram shows. It is a basic On-Off switch. An example which uses a single pole, single throw switch is a flashlight.  When a user presses the power button, the circuit is completed and the light turns on.

PTM Veröffentlicht am: