Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
power-switch-slide2

The most common range for power switches is between 48V and 277V.  Within this range, there are three typical power levels. In a low power switch, users will be switching less than 2A at the rated voltage. In a medium power switch, they will be switching greater than 2A and less than 10A at the rated voltage. In a high power switch, they will be switching above 10A at the rated voltage.

PTM Veröffentlicht am: