Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Detectors-Slide18

The choice of an RMS responding detector will generally begin with a narrowing down of the available options based on the required input frequency or input frequency range. The second most important specification will be the power detection range of the device which can range from 30dB to 65dB. The final device selection can then be made based on temperature stability, power consumption and package size.

PTM Veröffentlicht am: