Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Detectors-Slide12

To perform the calibration procedure, at least two RF power levels are set and the corresponding ADC codes are read. The known RF power level which comes from the external RF power meter, along with the asociated ADC codes are used to calculate the SLOPE and INTERCEPT which are then stored in the system’s non-volatile RAM. Once the system has been calibrated, it can be put into operation. The RF power meter is removed and the antenna is reconnected. To precisely measure the RF power, the ADC code is read and is combined with the known SLOPE and INTERCEPT in the equation RF Power = Code/Slope + Intercept.

PTM Veröffentlicht am: