Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
AS5047 Rotary Position Sensor Slide 17

In summary, the added values of the AS5047P, with DAEC™ can be summarized as follows. The AS5047P features ams OSRAM's DAEC™ (dynamic angle error compensation) technology, which produces outstanding angle measurement accuracy even at very high rotation speeds. Immunity against homogeneous external magnetic stray field is guaranteed. ams OSRAM's AS5047P is a low cost alternative to optical encoders that provides high accuracy performance in harsh environments. It enables customers to dramatically reduce system costs by replacing expensive high speed resolvers with a high accuracy, low cost, solid state angle measurement solution. The ABI outputs are equivalent to the outputs of a standard optical encoder, allowing designers to replace an optical encoder with an ams OSRAM magnetic position sensor measurement system, without any change to the control software or interface.

PTM Veröffentlicht am: