Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Introduction to Wi-Fi Technology Slide 18

TCP/IP is a set of communications protocols used for the Internet which specify how data should be formatted, addressed, transmitted, routed, and received at the destination. Another component called the Configuration Utility allows users to set up system parameters like security and access point settings. At the beginning of the presentation it was mentioned that WLAN is essentially wireless Ethernet. WLAN and Ethernet drivers connect to the TCP/IP stack and the Configuration Utility in the same way. This allows Ethernet-based products to be upgrade to a wireless connection without needing to rewrite the software.

PTM Veröffentlicht am: