Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Introduction to Wi-Fi Technology Slide 17

Another factor to consider when it comes to signal quality is coexistence. The wireless spectrum, as previously discussed, is crowded within the 2.4 GHz band. However, there are also other devices operating outside of this band which include GPS, GSM, 3G, and WiMax. The issue is that among all these standards, there is no established cooperation which can lead to interference. This can be solved through RF isolation such as shielding or filtering. There can also be coexistence issues inside a device when multiple RF technologies are operating simultaneously such as in combo chips with GPS, Bluetooth and/or Wi-Fi capability. This can also be solved through RF isolation between different bands and coordination in the same band in the case of Wi-Fi and Bluetooth both operating at 2.4 Ghz.

PTM Veröffentlicht am: