Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Introduction to Wi-Fi Technology Slide 10

Aside from Wi-Fi certification, there are also regulatory certifications to consider. Although, Wi-Fi operates on the unlicensed bands of 2.4 GHz and 5 GHz, there are still regulations that apply because Wi-Fi devices are classified as intentional transmitters. Depending on where the device will operate, it may need to adhere to regulatory bodies such as the FCC, IC, CE, ETSI, or TELEC as well as undergo compliance testing which can cost up to $25,000.

PTM Veröffentlicht am: