Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
I2C and SMBus Solutions Slide 9

Texas Instruments, has a variety of I/O expander products. These are shown in the parametric table in this slide. The y-axis is the number of I/O pins which the device interfaces with, and the x-axis is grouped into reset pins as well as internal or external pull-up resistor configurations. More recent devices are shown in red. For example, if a customer is looking for an 8-bit I/O expander with a reset input, and it must be low power; something like the TCA6408A might be the best product choice.

PTM Veröffentlicht am: