Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
I2C and SMBus Solutions Slide 13

The I²C Buffers and Repeaters can provide I²C bus expansion and can successfully extend the line capacitance to greater than the 400 pF capacitance limit that is dictated by the standard I²C protocol. This is done without any degradation of system performance. In addition to this, since all I²C devices require a unique I²C address, address conflicts can arise. Through the use of a buffer or repeater, this issue can be resolved.

PTM Veröffentlicht am: