Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
I2C and SMBus Solutions Slide 5

The figure in this slide is of a typical I²C bus with the master device, which is typically a processor, and multiple slave devices linked to the I²C bus, each possessing a unique I²C address. The I²C bus supports a maximum bus capacitive load of 400pF. This load includes all I²C devices as well as trace lengths. As the system block diagram illustrates, there are many different devices that can connect to the I²C bus. TI has products and content in all of the areas shown in either red or blue, but this presentation will be highlighting the products shown in blue.

PTM Veröffentlicht am: