Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
firm update
The RX65x family with high density memory supports both linear and dual flash memory mode. Dual mode allows for on-the-fly firmware updates using the background operation function (BGO). In this example, existing firmware is executed in Bank 1 while new firmware is loaded into Bank 2. The Bank 2 area can be selected via an address swapping function, and upon reset, the new firmware will start executing.
PTM Veröffentlicht am: