Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
hi end mig
RX651/RX65N is designed to fill the performance gap between the legacy 100 MHz RX63N/RX631 and the flagship 120 MHz RX64M, which contains up to 4 MB of flash memory. The RX651/RX65N has 50% higher performance with 60% lower power vs. the RX63. Using the Renesas Firmware Integration Technology, or “FIT”, customers can easily migrate their applications from one MCU to another.
PTM Veröffentlicht am: