Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
large part
Displayed in the graphic on the right-hand side of this slide, the RX65x high-density products have 640 kB of RAM partitioned into separate 256 kB and 384 kB areas. The dedicated 384 kB of RAM enables the RX65x family to drive a TFT display without the need for external memory, and also frees up CPU resources, which is critical for embedded applications that perform multiple tasks at the same time.
PTM Veröffentlicht am: